STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G474 UART4 RX pin pull up

In STM32G474 UART4 pin no PC11(Rx) is 5 Volt tolerant . If I pull up this pin to +5V with 4.7kOhms then it will affect life or operation of microcontroller? please Suggest.

TIM14 OC1 Trigger into TIM2 on STM32G071

Hi,  Has anyone managed to Trigger Timer 2(Combined PWM Mode, One-Pulse) with Internal Trigger 3(ITR3). The TIM14 OC1 waveform is the trigger. When I run Timer 14 in output compare mode, with an active level on match between Couner and CCR1. I cannot...

danielbathtub_0-1762846429156.png danielbathtub_1-1762846482415.png

Resolved! Unrecognized device markings

I can't decipher the silkscreen markings on this chip. Could you please help me confirm?This chip looks like it's from ST, but I didn't see the ST logo. I suspect it's an abbreviation for STM32G473ME, but I can't confirm it, and the chip's datasheet ...

微信图片_20251111104846_1_301.png
topgunZh by Associate
  • 584 Views
  • 2 replies
  • 0 kudos

STM32U5G9 TrustZone MPCBB

I'm working with the STM32U5G9, trying to configure access to internal RAM blocks with TrustZone enabled.  Part of this configuration uses the HAL_GTZC_MPCBB_ConfigMem() function from stm32u5xx_hal_gtzc.c from STM32CubeU5 v1.7.0.I see in that functio...

rdl_42_0-1760045616550.png
rdl_42 by Associate III
  • 780 Views
  • 3 replies
  • 1 kudos

Resolved! NUCLEO STM32U575ZI-Q USB Device CDC Problem

Hello, I am trying to use the STMicroelectronics classic USB device middleware to implement a CDC class in the STM32U575 microcontroller. I am currently working on NUCLEO-u575ZI-Q. At first, I followed the tutorial on "How to use STMicroelectronics c...

IlariaCrupi_0-1709029783341.png IlariaCrupi_1-1709029800660.png IlariaCrupi_2-1709029817595.png IlariaCrupi_4-1709029965795.png

STM32 G071 full erasing problem

I am uploading a custom bootloader to an STM32G071. When I select Full Erase, I get the error "Error occurred during mass erase." How can I solve this? I am using Utility.   

Afsal by Associate
  • 378 Views
  • 1 replies
  • 2 kudos

Blanco stm32h757 programming first time.

Hey,I have an STM32H757 that I’m trying to program for the first time.When I try to program it using STM32CubeIDE or CubeProgrammer, I lose the ST-Link connection after programming one of the cores.Changing the programming order doesn’t solve the iss...

MVops by Associate
  • 548 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.