STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

board power consumption (L0, v3pwr, nucleo stm32l053r8)

Questions are at the endI did some measurements with nucleo stm32l053r8, stlinkv2 cut off, led3 removed power supply form v3pwr via3.3V cn6 pin4GND cn6 pin6Tools used stm cubemonitor power v1.2.1 & stlinkv3pwr multimeter (should still count as factor...

_richard_0-1693381328910.png
_richard by Associate III
  • 4778 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G4 series - I2C2 SDA and SMBA in datasheet switched?

I just noticed the following:In the datasheets for the G473 and G483 the pin table and alternate function table disagree which pin has the I2C2_SMBA and I2C2_SDA function.The pin table claims PA10 is I2C2_SMBA and PA8 is I2C2_SDA. The alternate funct...

AF_table.png pin_1.png pin_2.png
Loebl by Associate II
  • 3971 Views
  • 4 replies
  • 4 kudos

I2C Slave interrupt mode not behaving as expected

Hi All,I need some help with setting up a I2C slave on a STM32L422 chip. I have tried following the example: STM32Cube_FW_L4_V1.18.0/ NUCLEO-L412RB-P/examples/I2C_TwoBoards_ComIT but it doesn't seem to make sense to me. I realize it is not exactly th...

IR TRANSMITTER

I was wondering if I could find any library for simulating IR signals with an STM32 microcontroller. I couldn't find any library for this purpose. While I did come across some work done by Controllers Tech on receiving IR signals from a re...

skuma.8 by Associate III
  • 3124 Views
  • 3 replies
  • 0 kudos

Resolved! Dual bank execution from Bank2 (STM32L071)

Hi,According to some of the on-the-fly firmware update documents, update is done with the following steps:- program the new firmware to Bank2- set BFB2 bit to start executing from Bank2- while in Bank2, copy the code from active Bank2 to Bank1- reset...

zoranr_0-1692304046755.png
zoranr by Associate II
  • 4447 Views
  • 3 replies
  • 1 kudos

Resolved! Timer waking from Sleep mode

MCU is writing data to ext flash once every 15 minute. I have set Timer in interrupt mode with one minute callback and incrementing the flag. In main while loop, the flag is being check . Once flag has reached 15, the MCU writes data to ext flash and...

Nico3 by Senior
  • 5732 Views
  • 9 replies
  • 4 kudos

Resolved! STM32H5 ADC, Multiple Channels, Continuous Scan, Interrupts

New to this ADC...I intend to call  HAL_ADC_GetValue() from HAL_ADC_ConvCpltCallback().How do I know which channel the conversion is for? Must HAL_ADC_ConvCpltCallback() keep track of the channel, trusting the ADC HW to follow the same channel orderi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.