2023-09-20 10:05 AM
Hello,
I tried copying BSP and Utils folders from "Repository/STM32Cube_FW_F4_V1.27.1" into my project, I included them in "Paths and symbols" project settings too.
When trying to build the code, I encountered a lot of compiler errors of symbols not being defined, for example symbols like:
- DFSDM_CHANNEL_SPI_FALLING
I then attempted to edit the "stm32f4xx_hal_conf.h" (following advice from this thread) and uncommented the following line:
/* #define HAL_DFSDM_MODULE_ENABLED */
Now I'm facing bunch of errors due to lack of "stm32f4xx_hal_dfsdm.h" file which I can't find anywhere.
Is there anyone who can successfully use BSP lcd functions for the STM32F412G-Discovery board and would be willing to share what is the process of getting it to work using STM32CubeIDE?
I attached the file I'm trying to compile in case if anyone would like to take a look.
Solved! Go to Solution.
2023-09-22 7:23 AM
Removing the following files from Repository/STM32412G-Discovery directory fixed the problem:
- stm32412g_discovery_audio.c
- stm32412g_discovery_audio.h
2023-09-22 7:23 AM
Removing the following files from Repository/STM32412G-Discovery directory fixed the problem:
- stm32412g_discovery_audio.c
- stm32412g_discovery_audio.h
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.