STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM DMA settings

Hi there, i am using STM32F401RE development board and using PWM generation using DMA. I am following register level programming approach and here the issue lies in the DMA settings. Like if I set my PSIZE and MSIZE to 32-bit long and also if my data...

DJ1 by Associate III
  • 3427 Views
  • 5 replies
  • 2 kudos

NUCLEO-H743ZI2, Unknown USB Device

 Hello,I'm attempting to set up the CN13 USB port as a Virtual COM Port (VCP) for transferring data to LabVIEW. Unfortunately, I'm encountering an error message that reads "Unknown USB Device (Device Descriptor Request Failed)." I've already installe...

image_2023_09_26T13_36_43_009Z.png image_2023_09_26T13_36_43_009Z.png

FMC: How to delay chip select?

I should combine STM32F479 with PROFIBUS-DP ASIC SCP4-2 The chip is aged. And requires delay of at least 30ns (by 3v3) between address and cs. Our previous design was based on SAM4S and their CPUs are offerring register to program such delays. In STM...

2023-09-25 10_32_07-Window.png
AlexKern by Associate II
  • 3655 Views
  • 4 replies
  • 1 kudos

STM32G4 Reset Issue

I am having some strange power up (I think) issue with my STM32G431 controller.  Sometimes it runs for a second or two, sometimes nothing.  It will usually not connect via the SWDIO pins so it is difficult to step through in debug to see where the pr...

STM32G4 Schematic.jpg

Resolved! UART Receive code is not working.

I am using STM32F103C8 MCU and Trying to communicate with Quectel EC200U-CN 4G module and i am not getting data through UART2 Receive pin. Please go through my code and suggest mevoid USART2_IRQHandler(void){ if ((USART2->SR & USART_SR_RXNE) != RESE...

Siva Ram by Associate II
  • 3498 Views
  • 5 replies
  • 1 kudos

PowerSTEP01 example code and programmer user guide

Hi, i m trying to program PowerStep01 with SPI on STM32H7, can anyone kindly advise where to locate sample code and tutoral ? or programmer user guide?  A serach online yield this but error on page and file not found. https://my.st.com/content/my_st_...

Resolved! USB on-the-go high-speed (OTG_HS) - core setup confusion

In RM0456 section 73.4.3 OTG_HS core (p.3279) I found the following statement:"The OTG_HS receives the 60 MHz clock from the reset and clock controller (RCC). This is typically generated in the PLL associated with the HS PHY and enabled in the RCC. T...

TDJ_2-1695126149597.png TDJ_1-1695125909206.png
TDJ by Lead
  • 14379 Views
  • 5 replies
  • 2 kudos

What lead times and deliveries are you seeing?

Sorry to bring up the elephant in the room. I just reviewed the ST Q1 quarterly results from April and was astonished to not find anything related to lead times, shortages, or allocations.My company is in the Musical Instrument space. We work with a ...

AHigg by Associate II
  • 5200 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.