STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Battery charger using stm32 & ltc4015

Hi currently I am implementing a smart battery charger using stm32 & ltc4015.But i could not understand how to perfectly configure ltc4015 through i2c protocol.So could you please inform me how to write the i2c sequences to safely charge the battery....

STM32G431 one pulse mode

Hello everyone,I am unable to understand how to get one pulse . Tried methods from online but cannot get any result. I only see a sine pulse from the terminals in oscilloscope.I would like to give a pulse of 15 V and 3A for 50 micro seconds to my 3 p...

Kv.2 by Associate
  • 1383 Views
  • 1 replies
  • 0 kudos

STM32G483 ADC Noise when connected to OPAMP PGA Gain -3

Hello,we use a STM32G483RE for analog sampling of downconverted RF signals. To maximize the signal-to-noise ratio in the digital domain we use one of the OPAMPs in inverting PGA mode with a voltage offset that is fed by a differential to single-ended...

gefa_0-1696582303316.png
gefa by Associate
  • 1764 Views
  • 0 replies
  • 0 kudos

SWV not working with STM32F469I-DISCO

I'm using a 32F469IDISCOVERY board (Cortex-M4). The integrated ST-Link V2-1 has firmware V2J37M27 and is configured as "Debug + Mass storage + VCP Modus" (default). It doesn't look like it has a jumper or solder bridge to connect SWO and I think it's...

AWebe.1 by Associate
  • 3793 Views
  • 2 replies
  • 0 kudos

Rewiring PF2-NRST to GPIO - Does this brick SWD debugging?

Hello, I need the PF2-NRST pin on the STM32G0C1 chip as an MCO. Thus, I had to change the user flash to use the pin in GPIO mode. While I had doubts about this approach's validity since we are fiddling with the NRST, I still went ahead with it. Now t...

NGall.5 by Associate II
  • 3283 Views
  • 4 replies
  • 1 kudos

Resolved! stm32g030 not flashing

i'm trying to read the G030 mcu (from my PCB) with cubeProgrammer and the results are:"No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication"Today the debug pins are direct connectio...

WBria1_0-1696475699047.png
WBria.1 by Associate II
  • 5834 Views
  • 9 replies
  • 1 kudos

Program hangs after calling HAL_UART_Transmit_DMA

Hi,I'm using AzureRTOS on a STM32H743ZI. I have a low priority task that is sending data via UART every 100ms (115200 baud). I would like to send this data with HAL_UART_Transmit_DMA, but after calling this function, the program stucks in the functio...

KR51K by Associate III
  • 1297 Views
  • 1 replies
  • 0 kudos

STM32f205vet6

I am using STM32f205vet6 in that there is no availability of sub seconds Iam using rtc based timer and also I have code for stm32g0 series for that when I try to migrate the stm32 G0 code to F2 series error are happening I a way to migrate the same c...

AKHIL6 by Associate II
  • 1799 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.