STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to program STM32F103 through UART

I created a custom board with the STM32 (F103C8T6), and I am trying to program it using a FTDI USB to Serial module. However, nothing is happening, it doesn't seem to be sending anything and when I try using STM32CubeProgrammer it says:Timeout error ...

Nv7_2-1694149065260.png Nv7_4-1694149113730.png
Nv7 by Associate III
  • 11350 Views
  • 13 replies
  • 1 kudos

CODEC with STM32

Hello, I would like to know how to retrieve the acquisition values ​​: INPUT -> ADC -> SAI -> µP like the diagram below : I have a program that works for this : DMA -> SAI -> DAC But this is not the way I would have wanted to make my CODEC work. Do ...

DYann1_0-1692602441481.png
DYann.1 by Senior II
  • 14226 Views
  • 30 replies
  • 0 kudos

Migrating from Nucleo-144 board to real IC

HI i m currently working on a H723 nucleo144 EVK, and have completed the coding and is contemplating to flash the code onto STM32H750IBK6. Question is whats the best way to port over the code (with .ioc) without recreate a new project,  new IC select...

Resolved! Blocking vs non-blocking UART using an RTOS

Hello there!I've been setting up the UART peripheral on my STM32H5 and everything works great! However, there is one thing I can't completely understand:Using an RTOS to call HAL_UART_Transmit or HAL_UART_Transmit_IT, what's the advantage of one over...

nunokisi by Associate II
  • 7768 Views
  • 4 replies
  • 1 kudos

Didn't get the same binaries with the same compiler

Hi everyone,I'm currently trying to build my project on two differents computers. My computers have not the same STM32CubeIDE: 1.13.1 and 1.11.2. Compilers are the same, I ckecked it with version 10.3-2021-10. Flags and options of compilation are the...

HAL_DAC_Start_DMA doesn't correctly display audio.

I wanted to use DAC with DMA with TIM5 being the trigger. my problem is that it does not correctly display the audio,I mean the original audio is like 10 seconds, I first tried to do the transfer by the CPU so that for every interrupt generated by th...

abdosalm_3-1697806359225.png abdosalm_4-1697806363614.png
abdosalm by Associate II
  • 2497 Views
  • 3 replies
  • 1 kudos

STM32F4 UART DMA

Hello all,I have a project using UART DMA for receive datas from Nextion HMI. When i touch a button on Nextion Screen, data should be received a buffer via UART DMA.  First five hour it works good but after five hours no data flows. It is like the bu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.