STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 Bootloader firmware write over uart

Hi everybody,I'm working on a project where I have a pi cm4 connected to a STM32 (during testing we're using a STM32G07 dev board, but production will be using an STM32G03 chip). I've been asked to write a program to allow the cm4 to update the firmw...

jbreaper by Associate II
  • 6450 Views
  • 9 replies
  • 5 kudos

Issue coming out of standby mode using RTC

Hi I am having issues coming out of standby mode using RTC timers. I am using both timers and the periodic counter, all at different times. If I dont go into stanby mode all works as expected, and the interrupts are generated for each clock and timer...

Programming internal flash

I´m about to use the STM32L471xx circuit and want to program it from an external source.What type of interface can I use to program the device?I want to avoid using the JTAG interface.Is it possible use USB or SPI interface?

Andreas3 by Associate
  • 1979 Views
  • 3 replies
  • 2 kudos

Resolved! How to make standby mode pin stay low

I am using stm32f302r8t6 microcontroller. In standby mode, the pins on port A are high, which should not be the case for the card I designed. For the stm32f302r8t6 microcontroller, I should keep one pin on port A low in standby mode.

YBAYR.1 by Associate III
  • 2935 Views
  • 4 replies
  • 2 kudos

How can I set the timer to trigger ADC on counter overflow?

Hi, I have set the timer4 in center alligned mode 3 and I want to trigger ADC on counter overflow. If I understand correctly the ADC trigger input TIM4_TRGO can be set in timer configuration as update event output but that means also in underflow wil...

NTosi by Associate III
  • 4948 Views
  • 10 replies
  • 0 kudos

Anomaly list for peripheral library

Hello,We use standard driver libraries for STM32F10x and STM32F4xx. Looking for list of bugs reported on these. The previous link doesn't seem to exist anymore https://community.st.com/s/topic/0TO0X000000BWVLWA4/bugreport.Please help in getting the n...

BT by Associate
  • 1904 Views
  • 3 replies
  • 0 kudos

Resolved! Generate a specific PWM signal

Hi ST community,For a project I would like to generate two interdependent PWM signals (Sa and Sw in the attached figure) with the STM32G0. The constraints/tasks are as follows:tSw,off = constant for ~100nstSw,on = in a time range from ~100ns to 20us ...

Resolved! STM32 Controlling Resources via JTAG/SWD

I there a way (device or API) to control STM32 resources via JTAG or SWD without the need to downloading a custom program?  For example, setup GPIO pin with pull-up and direction and then write value.  In addition, be able to perform more advance sce...

NotSure by Associate II
  • 5710 Views
  • 8 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.