STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Web Browser on RTOS.

Hello, I want to know if it is possible to run web browser on RTOS prefferably on FreeRTOS. I tried the using QT but could not get any lead. Please let me know if you are aware of such browser that can run on RTOS, of at least steps by which I can ru...

Need Help to understand this code

this is code from an Udemy tutorial but i couldn't get the part of 9 bit data transfer with no parity bit can anyone help me to understand that please 

Screenshot 2023-10-12 195942.png
Asraful by Associate III
  • 8088 Views
  • 18 replies
  • 4 kudos

STM32H7 DFU jump to application doesn't work

Controller: STM32H743ZIT6Custom BoardSTM32CubeProgrammer, STM32CubeIDEHi, since a few months we have an issue with flashing our Microcontroller application.We are using automatic firmware flashing over DFU-Util on a Linux based system, which is conne...

PStoc.3 by Associate II
  • 3406 Views
  • 4 replies
  • 1 kudos

Resolved! Delay with timers(Non blocking delay)

Hi,I need  microsec/millisec delay  in my project but I don't want to effect the process flow.I am using STM32G4.I am using timer for microseconds delay below is the function.void delay_us (uint16_t us){__HAL_TIM_SET_COUNTER(&htim1,0); // set the cou...

Resolved! RNG does not work after waking up from the stop mode

Hello,My MCU is STM32L053R8I use freeRTOS project generated by CubeMX.The problem is happening only  when I enable tickless sleep. I get only one correct reading, which is probably generated right after MX_RNG_Init. Then after the sleep, I always get...

Evgeny M by Associate II
  • 2936 Views
  • 2 replies
  • 2 kudos

STM32H723ZG AZURE RTOS - Hard Fault Error Regarding

As we are using STM32H723ZG-CT6 for our Medical project. We are using STM's Complement to STMH7 series - Azure RTOS for our project. We were runs totally 8 threads, during the running time of threads Hard fault error is coming and our controller stop...

Screenshot 2023-11-27 190422.png
rkuma.21 by Associate III
  • 2421 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.