STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5 I2C

STM32U5  + LSM6dslI want to read the general accelerometer register of the I2C interface.I think it can be achieved by using HAL_I2C_Mem_Read ().I set the second argument DevAddress to the value of the accelerometer slave address shifted left by 1 bi...

caiChangKun_0-1701166262232.png

Resolved! unexpected register change TIM1->DIER / interrupt enable flag

Controller: STM32G431VBT6Compiler: arm-none-eabi-gcc version 12.2.1Libraries: CMSISI use STM32G431VBT6 for a sensorless BLDC motor control with zero-cross detection.TIM1 is used for PWM outputs. See below part of the code. RCC->APB2ENR |= RCC_APB2ENR...

Marc1 by Associate III
  • 3001 Views
  • 8 replies
  • 1 kudos

Resolved! flash memory write problem

hello experts ,my device is stm32f103c8t6 ,cubeide 1.14.0it shows 64kb flash in ide but shows 128kb in stmcube programmer ,my issue is if i write flash from inside the programme while mcu running then it writes fine but when i erase the page and try ...

ahmash by Associate III
  • 3288 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F030R8 PWM to LED (PA5)

Hi all, I am looking into generating a PWM signal using the Timers and route it to the PA5 pin to blink the LED, but PA5 does not have a TIM routed to it. I thought about just having a timer work in my code and toggle the pin every second by checking...

tolgaust_0-1701193381887.png
tolgaust by Associate II
  • 2304 Views
  • 2 replies
  • 2 kudos

Resolved! RTC SCHEMATIC

Hi,I need RTC LSE schematics and ETHERNET output schematic for STM32H563ZI, where can I find them, I am searching but It directs me to datasheets that don't have schematicsThanks for your answers.

Recep by Associate II
  • 1961 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.