2023-10-12 6:56 AM
Controller: STM32H743ZIT6
Custom Board
STM32CubeProgrammer, STM32CubeIDE
Hi, since a few months we have an issue with flashing our Microcontroller application.
We are using automatic firmware flashing over DFU-Util on a Linux based system, which is connected over USB to our STM32H7 custom board. We use the ST propritary Bootloader over USB DFU which is preinstalled.
After installing the firmware the device should jump into application with the following command:
$dfu-util -a 0 -s 0x08000000:leave <location-to-binary>.bin
That doesn't work.
What we have tried:
Workaround:
After flashing the controller we make a hard reset, the application starts as usual.
Possible solution:
The error no longer exists with the latest Boards we produced. To examine the difference between old an new boards, we reviewed additional boards and noticed that older ones have bootloaderversion V9.0 installed and new ones V9.1
Question:
Is it possible that any sideeffect of the fixes in V9.1 fixes our problem or is the AN2606 not up to date?
2023-10-17 1:12 PM
Hello @PStoc.3,
The problem here might be related to this post: DFU mode with system bootloader is not working, wh... - STMicroelectronics Community
STM32H7 System Bootloader sometimes not working.
Imen
2023-10-18 5:35 AM
Hello @Imen.D ,
thanks for your reply. This two topics I haven't seen before and they are a good hint.
But I think the topics doesn't fit as good, because the most DFU-commands works reproducibly and stably. Only the DFU-leave command doesn't jump to application.
2023-11-28 1:33 AM
Hi,
have you found a solution?
I have the same issue.
I'm using a STM32H723 controller and the dfu leave doesn't seam to work.
The dfu bootloader is exited, but the applicaiton is not started.
2023-11-28 1:49 AM
Hi.
sry: uncommenting USER_VECT_TAB_ADDRESS fixed my issue
#define USER_VECT_TAB_ADDRESSfixed my issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.