STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 HS USB CDC Serial, not recognized by Windows

Hello,We have a custom board design using STM32F765IITx processor. Trying to configure and generate a working project using the HS USB interface with an external PHY. (USB3315) The project being generated is for Keil (MDK-ARM)The latest versions of S...

Resolved! How to use virtual COM port with nucleo-H563ZI

Hello,I am new in the STM world.I am using the nucleo-H563ZI deverlopment board and I want to get the virtual COM port to work.On github I found the examples of the Board.https://github.com/STMicroelectronics/STM32CubeH5 I opend the project "...\Proj...

STM320L0 I2C timing issue?

I'm working on a board with a STM32L010K.For some reason, I can't get the I2C code to work properly. I mean it works (data gets read from the slave) but not if a lot of things are done in succession, then a hard fault is thrown.Below is the block rea...

The strange GPIO pullup output voltage

I tried 3 boards F407vet6 x2 and F427 x1.I found both pullup and pulldown gpio output in PP and OD will put a low voltage. 20mV in down and 50 mv in up.This situation is based on the stdperiph-LibHowever, use the Hal-Lib to implement the gpio output,...

Rian by Associate
  • 2351 Views
  • 2 replies
  • 2 kudos

STM32H7 USB Audio as USB device class

Hi everyone,in my latest PRJ, i had to run some arbitrary waveforms. The idea was to connect my STM32H7 to the host and configure it as USB audio device. As far as good...the problem is that i had to drive 60kSps (16Bit). So since i've read on the X-...

Internal JTAG on STM32

Hello all together! :)Does anybody know if an internal JTAG device is integrated on the STM32H562 oder STM32H563?In my case, I need to implement the functionality to flash an external microcontroller over the STM32 chip itself.That would mean, I have...

Low power on STM32L4 series using RTOS

I've been trying to implement low power modes on an STM32 L496 (Nucleo board) while using RTOS. I've tried with both freeRTOS and ThreadX. I followed official ST articles/tutorials and the lowest I got so far has been ~250 uA.  So, has anyone been ab...

Ans by Associate III
  • 4896 Views
  • 5 replies
  • 0 kudos

What SDIO interface chip (with a 3.3V host side) are people using these days? The IP4856CX25 (used on the H7 Eval board) is NRND.

What SDIO interface chip (with a 3.3V host side) are people using these days? The IP4856CX25 (used on the H7 Eval board) is NRND, and I can't seem to find an SDIO interface chip that supports a 3.3V host side. What part should I use for a 3.3V H7 des...

chriscole by Associate III
  • 7084 Views
  • 10 replies
  • 1 kudos

SPI CS unable to pull to high initally

Hi I m using STM32H7 for SPI transmit & receive, the code is working and able to transmit 2 byte successfully as seen from scope, but the inital CS pin was unable to set to high from .ioc. CS = PA4 and set to GPIO output level HIGH and max output spe...

CS not lo.jpg

Resolved! Confusion in understating the FLASH STRUCTURE OF M4

Hii thereI am using STM32F410RB (M4). it has a flash of 128 KB divided into following 4  sectorsMy query is that I want to store and retain some non-volatile data in the flash. We can use the last few pages of the flash for this purpose. I have come ...

skuma8_0-1701225308073.png
skuma.8 by Associate III
  • 5203 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.