STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401RET6 RTC initialization failed one power up

Hi,The RTC block was driven by LSI (internal RC osillator), we just found few boards failed to initialize the RTC block and the program was stuck there. What could be the possible reason? Is it due to the floating pin of Tamper?thanks,Qi

QiWang by Associate
  • 1191 Views
  • 1 replies
  • 0 kudos

STM32F401RET6 failed UART communication

We just found few boards failed UART communication. The debug process for this issue points to the LSI and RTC block inside the MCU STM32F401RET6. The RTC block was driven by LSI (internal RC oscillator), these boards failed to initialize the RTC blo...

NealXu by Associate
  • 1356 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F407 CAN Loopback Mode work but Normal Mode not working

Hello, I am trying to establish standard CAN communication between the sn65hvd230 IC and the stm32f4 discovery and stm32f103. While the loopback mode works fine, when it sends data to the normal mode, the output goes to 0 and then back to 1. I still ...

Sergen by Associate III
  • 11185 Views
  • 11 replies
  • 0 kudos

STM32L432 Nucleo board: ADC has -53 mV input offset ?

I'm using a STM32L432KC Nucleo board, and reading a voltage with the 12-bit ADC. On this board the ADC Vref is connected to the board 3.3V, which in this case actually measures 3.315 V.  With a 12-bit resolution, I would expect that 4095 ADC counts =...

JBeal.1 by Associate II
  • 2644 Views
  • 4 replies
  • 0 kudos

STM32L073 datasheet incomplete information

Hi,As per DS10685 Rev 7 (https://www.st.com/resource/en/datasheet/stm32l073v8.pdf), there are so much information missing, for example:1. Table 17 doesn't mention that the USB pins D+ and D- are bound to PA11 and PA12 ports, respectively, but Table 1...

XR.1 by Senior
  • 1637 Views
  • 2 replies
  • 1 kudos

Resolved! STM32L476 SPI3 Using DMA2 Chan 2. No Transmit.

Hello Everyone. My how the forum has changed. Just dropping a recent odd experience here to see if anyone might have any comments. No. I don't use CubeMx and no this isn't another 3 year anniversary item regarding initializing the DMA before any peri...

Octospi vs FMC

Hi,I am doing a new design of a board and I am wondering what is better to have as in interface for a external memory FMC or Octospi? Thank you

aabba.1 by Associate III
  • 4789 Views
  • 2 replies
  • 2 kudos

Resolved! STM32CubeIDE 1.13.2 not showing X-Cube-Mems1

Hi All,I have configured for STM32L071xx xx controller bare metal. I was not able to find X-Cube-Mems1 for the controller.Please me know if LIS2MDL (or Mems package) is not supported on STM32L0 series?PFA screen shot of the STM32Cube IdeThanks,Milind

mvk by Associate
  • 1677 Views
  • 1 replies
  • 0 kudos

Resolved! RTC clcok slow when turning on LTDC

Hi,I am using a custom board to do some application (https://www.waveshare.com/openh743i-c-package-b.htm). On this application I should turn on LTDC (to use it with touchgfx) and I am also using the RTC.When I am only using RTC alone, the RTC clock i...

aabba1_0-1702234030670.png
aabba.1 by Associate III
  • 1646 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.