STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Having Issues with ADC configuration STM32L011K4T6

Hello,  I have tried for the last couple of days to get use 2 pots to change the frequency and duty cycle of a PWM signal using "Bare Metal" programming due to the flash limitation of the STM32L011K4T6 I rapidly ran out of space using HAL and was not...

Triggering SPI DMA transfer with TIM1 event.

Hi everyone,I am using STM32F410 CPU.I need to send 4096 bytes of data via SPI using DMA transfer.The transfer should be triggered by each TIM1 event.I have read these two posts:https://community.st.com/t5/stm32cubemx-mcus/trigger-spi-dma-transfer-fr...

load2005 by Associate III
  • 2637 Views
  • 3 replies
  • 0 kudos

Elf loader is bigger than RAM size

Hello I am using STM32L010k4 controller for one of my project. And I am trying to program using stlink utility. My binary file size is 7.5kb. - my controller is successfully connected from utility- I can successfully erase chip by stlink utility But ...

Resolved! I was Unable to use RTR(Remote Transmission Request) in CAN using STM32F407VGT6 and STM32F302R8

I tried to send a RTR frame to another CAN peripheral , another node received the RTR bit successfully and RTR bit in the node has been set. Does the node receiving the RTR frame will transmit the Message automatically? or We have to read the RTR bit...

CAN question with STM32F103C8T6.

Hi all!,I have 2 STM32F103C8T6 connected by CAN bus.Each STM32F103C8T6 has the same firmware.This firmware starts sending a message "RequestID" by the CAN bus.Is there a way to avoid send the "RequestID" in case another "RequestID" were detected on t...

JAlca_0-1699692973609.png JAlca_1-1699693190500.png
JAlca by Senior
  • 1488 Views
  • 1 replies
  • 0 kudos

Resolved! Issues with CANBUS on STM32F072: Bit Dominant Error

Hello,I am currently working to get CAN transmission to work on a STM32F072B-DISCO. I am continuously getting a BIT_DOMINANT_ERROR in the LEC of the CAN_ESR when attempting to transmit. I am using a TCAN1044 (https://www.ti.com/lit/ds/symlink/tcan104...

PF-JohnF by Associate
  • 4837 Views
  • 4 replies
  • 0 kudos

Lost debug messages from LORA WAM STM32WL device

I lost debug messages from my LoraWAN end device. I made some changes using MX on my project, and this way, I lost debug messages displayed on a serial wire monitor (for example, on Arduino serial monitor). I think it was the cause of this problem. N...

markpow_0-1703241149646.png
markpow by Senior
  • 4011 Views
  • 10 replies
  • 0 kudos

Resolved! STM32 with capsense support and ethernet available?

I've taken a look at AN5105 (Getting started with touch sensing control on STM32 microcontrollers) where they present a list with microcontrollers that support capsense:STM32F0 seriesSTM32F3 seriesSTM32L0 seriesSTM32L1 seriesSTM32L4 seriesSTM32L4+ se...

petervg by Associate
  • 2568 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.