STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4 TIMER INTERRUPT NOT HAPPENİNG

Hı everyone, ı was trying to design basic timer project in register level about toggling on related led pin every 1 second. However, the led is on a few seconds after that it is off and never becoming on. When ı do the same project in HAL library, it...

Resolved! STMH723 and LAN8742Ai PHY

Hi,I am working on a new product. For this I use the STM32H723 µC and the LAN8742Ai PHY from Microchip.Our schematics looks like this:We have a 25 MHz crystal connected to the STM32H723 (HSE). The MCO is configured to HSE. The crystal matches the clo...

Bild1.png
sada1400 by Associate II
  • 6018 Views
  • 8 replies
  • 3 kudos

USB FS Device parse_config_desciptors Error

Hello,I've enable a USB device as a virtual com port.  It works well however sometimes I get the following warning in CubeMX's console when I hit 'debug'.  The warning appears after I 'continue' after the first 'HAL_Init' debug break point."libusb: w...

LMorr.3 by Senior II
  • 1121 Views
  • 0 replies
  • 0 kudos

I2C doesn't work after uploading (only sometimes)

I wrote a little program that reads I2C values with interrupts: The Problem is that sometimes it just doesn't work after uploading. I just have to run it so many times till it works (not changing anything in the code). It seems like its just coincid...

Senax by Associate II
  • 5954 Views
  • 14 replies
  • 0 kudos

Resolved! Frequency PWM calculation vs real

Hi, I would like to understand why I don't have the right frequency on my PWM. I am working on STM32F103RG.I would like to have a 8Khz PWM on Timer 3 channel 1, so I have configure my HSI to 8Mhz. APB2 Timer is set to 8Mhz. Prescaler to 10 and ARR to...

ELECL.2 by Associate II
  • 3525 Views
  • 2 replies
  • 1 kudos

ADC DMA Doesnt Read Properly [Need Help and Advice]

Hi, so previously on other post I've been getting trouble with Poll Conversion of ADC using STM32F4 Discovery Board. Therefore i decided to use DMA instead.I made the program using STM32CUBEMX and Keil uVision to read 5 different channels. All data t...

watch1.JPG dma array output.JPG
dios_kuri by Associate III
  • 9314 Views
  • 13 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.