2013-01-17 12:34 AM
Hi Guys,
I am 1week old to stm32 programming I came from PIC1ST QUESTION // FROM Pic Basic Code normally I do this TrisC = %11111111 int data = PortC the return is the decimal equivalent of the binary or port C example 1000001 data will contain 65 then that is very easy to manipulate if you want to send via USART / LCD //00: General purpose output push-pull //01: Output mode, max speed 10 MHz. GPIOC->CRL = 0x11111111; GPIOC->CRH = 0x11111111; //10: Input with pull-up / pull-down //00: Input mode (reset state) // set as pulldown GPIOA->CRL = 0x88888888; GPIOA->CRH = 0x88888888; GPIOA->ODR = 0x0000; while(1) { GPIOC->BSRR |= GPIO_ReadInputData(GPIOA); //read pins and set PORTC from data of PORTA GPIOC->BRR |= GPIO_ReadInputData(GPIOA); //reset portC based from portA } this is working but i want to convert the data to 8 bit to represent an ascii i want a concept that is similar to this int data = GPIO_ReadInputData(GPIOA); instead of doing this: if (GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_6) == 1) { data +=64 } (GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_5) == 1) { data +=32 } (GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_4) == 1) { data +=16 } 2ND QUESTION usually in PIC to declare a input and output I DO THIS TRISA = %11110000 //1111input 0000output so port0-port3(output) port4-port7(input) so in STM32VL for example i want port A0 - portA7 as output and the rest A8-AX as input how do i do that?2013-01-17 2:21 PM
int data = GPIO_ReadInputData(GPIOA) & 0xFF; // Will mask low order bits
int data = GPIOA->IDR & 0xFF; // A more direct form The LCD code is done in a bitwise fashion to allow an agnostic implementation, where the pins are scattered, or in reverse order, or whatever. /* GPIOA Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /* Configure PA0 .. PA7 in output pushpull mode */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure PA8 .. PA15 in input, pulled up mode */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIOA->ODR = GPIOA->IDR >> 8; // Mirror high ordered inputs to low ordered outputs2013-01-17 4:48 PM
Hi Clide,
Thank you very much! your the best:) This gave me a good start to understand configuring pins in C. may I ask if you have a spare time this weekend and if you could give me a crash course just teach me how to start and that's it the rest I'll manage...:) I am trying to study on my own but it may stil take 2-4 weeks and my project is due this january 31. I hope you could be my mentor for at least 3-4 hours or for the basics of C in STM programming2013-01-17 5:18 PM
typedef struct
{ uint16_t GPIO_Pin; GPIOSpeed_TypeDef GPIO_Speed; GPIOMode_TypeDef GPIO_Mode; }GPIO_InitTypeDef; is this one GPIO_InitTypeDef GPIO_InitStructure; like creating an object of a class which allows me to use its variable or methods?GPIO_InitTypeDef - classGPIO_InitStructure - object / variable so I can make it something like GPIO_Initialization2013-01-17 5:28 PM
Please see if my understanding are correct
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; //will put implement the succeeding lines on the following pins 0, 1, 2,3,4,5,6,7 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; //will put implement the a 50 mhz cycle on pins 0, 1, 2,3,4,5,6,7GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; //will put implement a push pull on pins 0, 1, 2,3,4,5,6,7 GPIO_Init(GPIOA, &GPIO_InitStructure); //will implement all the setting above on portA //so if i have some thing likeGPIO_Init(GPIOC, &GPIO_InitStructure); settings above will //also be implemented to portC pins 0-7
2013-01-17 5:55 PM
type
structure GPIO_Init() is a function that takes a pointer to the structure (array in memory if you will) that contains the setting we want to apply.2013-01-17 5:57 PM
2013-01-17 6:04 PM
Thanks clive! how I wish you are the Philippines so I could treat you :) how about it clive do you have some spare time? could I have you as a mentor for few hours?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.