2023-08-29 5:33 AM
Hello,
I would like to design a microphone array with up to 16 microphones. I want to use the stm32h7a3zi board which has a lot of peripherals.
I was looking at the DFSDM interface, but with only 8 channels / 8 filters up to 8 pdm microphones can be handled.
On the contrary, the SAI interface seems to be more promising. If I understood correctly, the SAI interface can be configured as PDM interface, and every SAI can handle up to 6 microphones. Moreover, the SAI interface supports synchronization between SAIs modules.
Do you have suggestion/comments?
2025-06-10 7:19 PM
Hello, I know it has been 2 years since you posted this. But, by any chance, were you able to complete the project with SAI interface? I want to create a similar pdm arrary with less microphones.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.