2017-07-12 10:29 AM
This isn't really a question - since I found a solution. It's an observation in case others encounter a similar problem.
We purchased a new ST-LINK/V2 adapter recently and it shipped with firmware 'V2.J28.S6'.
We use this adapter along with a cable from Tag-Connect to program our boards (
STM32F030C8). However, I
found that I could only program our board if the cable was connected before I start the Program+Verify operation. (Related problem: the 'Automatic mode' does not recognize when the cable is connected to our board - and the utility gets sluggish when I do).Since the latest ST-LINK Utility included firmware version 27, I decided to 'upgrade' my adapter from 28 to 27.
Once I did this, everything worked as expected.
It would appear that ST-LINK/V2 firmware
V2.J28.S6 contains some kind of bug that does not exist in V2.J27.S6.
Anyone else seen this?
2017-07-13 4:34 AM
Hello
Seymour.Jim
,We cannot reproduce your reported issue using STLink/V2 with many boards and STM32F0308-Disco, tested with V2.JS6, V2.JS6 andV2.JS7(the latest on the ST site)
Which ST-Link Utility version and STLinkUSBDriver.dll are you using ?
Can you please describe clearly (in details) the steps that you have followed?
With Regards
Imen
2017-07-13 9:29 AM
I'm running ST-LINK v4.0.0.0; STLinkUSBDriver.dll 4.4.0.0; ST-LINK_CLI.exe v3.0.0.0. If it matters, this is on a Windows 7 Pro system (SP1; 64-bit).
Unfortunately, I can no longer duplicate the problem since I've flashed my adapter back to version 27. If you can point me to where I can get firmware 28, I can try to duplicate the problem again to provide more details.
2017-07-13 11:59 AM
28 should be in the ST-LINK Firmware Update
http://www.st.com/en/embedded-software/stsw-link007.html
2017-07-21 5:07 PM
I finally got time to play with this today - and I can duplicate the problem. If I program firmware 28 into my ST-LINK/V2, the 'Automatic Mode' in ST-LINK Utility v4.0.0 does not work. It does not recognize when I connect the Tag-Connect cable to our board.
As soon as I flashed the firmware back to 27, it started working.
If there's anything you'd like me to do to help diagnose this issue, I'm happy to help.
2018-01-12 12:16 AM
Tha same problem for me! The new S28 block automatic mode, but if i try S27 all works well! Please update the firmware! The Automatic mode is very useful!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.