STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LCD flickering issues & STemWin hardfaults.

Posted on January 12, 2018 at 13:55Hi,We are using a 216Mhz F7 (STM32F746NGH6) on a custom board to interface with an LCD (Winstar WF70GTIAGDNG0).  We are having issues with the screen flickering, often the screen will display a flickering green blo...

Resolved! SPI overrun

Posted on November 07, 2016 at 13:32 Hello everyone, I'm trying to read an external SPI flash using DMA but I occasionally get an SPI overrun error. I've managed to track down the error: I get no overrun errors when I disable the LTDC IRQ. And more ...

example with HAL_FLASHEx_Erase_IT

Posted on January 12, 2018 at 09:28hi, I know the way to use HAL_FLASHEx_Erase() in my main loop and it works,erasing some flash areas.Now I want to use the HAL_FLASHEx_Erase_IT() , I have enabled from the cube the flash global interrupt,Do I have t...

Apparent bug in ST-LINK/V2 firmware V2.J28.S6

Posted on July 12, 2017 at 19:29This isn't really a question - since I found a solution.  It's an observation in case others encounter a similar problem.We purchased a new ST-LINK/V2 adapter recently and it shipped with firmware 'V2.J28.S6'.We use t...

STM32F401RE-Nucleo Uart Problem

Posted on January 12, 2018 at 06:09 I'm using a stm32f401re-nucleo board and I build a project on ubuntu through arm-none-eabi-gcc compiler. Here is my code for uart. This code initializes uart. void UartInit(void) { hUart2.Instance = ...

HoYa Kim by Associate
  • 712 Views
  • 0 replies
  • 0 kudos

Resolved! NUCLEO F411RE USB

Posted on January 11, 2018 at 02:31Hello.NUCLEO F411RE, Workbench generated project, Ubuntu 64 16.04, STCUbeMX , I think is  V1.18I wired a USB cable to USB-DP (PA12)  USB-DM (PA11) GND and 5V.I have a usb initialised as simple as instructed.void MX...

Marius CO by Associate III
  • 1442 Views
  • 2 replies
  • 0 kudos

How set lowest speed for Canbus

Posted on January 11, 2018 at 21:22Hello friends,What is the lowest Canbus speed ? And how can I adjust the speedI need a Low and safe speedPlease guide meMCU = STM32F407ZET6 , HSE = 8Mhz , SysCLK 168MhzThanks for all of you

0690X00000609L7QAI.png
Pedram by Associate III
  • 1081 Views
  • 2 replies
  • 0 kudos

UARTS on a STM32L475VG Discovery board

Posted on January 11, 2018 at 23:10I have a Amazon Web Services example (AWS) example running on a STM32L475 Discovery board. I got the example from en.stsw-stm32078.zip and it in the C:\...\st Micro\en.x-cube-aws\STM32CubeExpansion_Cloud_AWS_V1.0.1...

STM32 and STPM33 weird SPI behaviour

Posted on November 22, 2016 at 20:52Hello,I'm building a multi phase power meter with 6 pcs of STPM33 ICs and an STM32. The STPM33 chips are on the same SPI bus, with separate chip selects (SCS) for each meter. The MCU can control all of the control...

holcsik by Associate
  • 4209 Views
  • 6 replies
  • 0 kudos

Resolved! Using stm32f4 on website

Posted on January 11, 2018 at 13:52 Hello I'm using stm32f411 and I have my server written in node.js. I want to make that my stm32 would send random string to my web server so it will be like a kind of a captcha when logging in. Is this eve...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.