2021-06-05 11:09 AM
Due to the current semiconductor shortage the microcontroller STM32H745ZIT6 is not available in the quantity of 210, so I had to buy the variant with higher temperature range. However, the data sheet says in small print that this variant does not support VOS0 and VOS1 operation, but I need this mode because otherwise I do not get the computing performance that I need. Is there a way to bypass this lock - it's ok if it makes the temperature higher, I don't need the high temperature range.
2021-06-05 2:57 PM
It's probably one of those things where the performance over the entire temperature range is just not guaranteed. It would be weird for them to disable it in the hardware, but I suppose it's possible.
2021-12-05 12:35 PM
I tried it and @TDK you are answer is correct, it works without problems with 480MHz!! Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.