2024-06-11 5:41 PM
I have this code it transfers to 0x90000000 (OSPI) data
__IO uint8_t *mem_addr;
/* USER CODE BEGIN 2 */
HAL_OSPI_MemoryMapped(&hospi1, &sMemMappedCfg)
mem_addr = (uint8_t *)(OCTOSPI1_BASE + address);
for (index = 0; index < BUFFERSIZE; index++)
{
*mem_addr = aTxBuffer[index];
mem_addr++;
}
it compiles and runs fine but freezes on *mem_addr = aTxBuffer[index];
has anybody seen something like this ?
2024-06-13 2:57 PM
I will just put it aside, enough fun for one day. I do not have similar problem with QSPI
I do not know why but if I read the memory address and write there then it works. Maybe something to take a look at later again.I tried all possible settings in CubeMX including lowering the clock.
mem_addr = (__IO uint8_t *)(OCTOSPI1_BASE + address);
for (uint16_t i = 0; i < BUFFERSIZE; i++)
{
dummy_operation[i] = *mem_addr; //without it programming does not work
*mem_addr = aTxBuffer[i];
mem_addr++;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.