2014-01-13 6:56 AM
I' m trying to save two ADC3 values in memory using dma, but nothing is stored in the memory, someone can help me, my code is:
int main(void) { //Configuration of the ADC channels used ADC_Config(); ADC_SoftwareStartConv(ADC3); printf(''start''); while(1) { //ADC_val=ADCConvertedValues[0]; if (ADCConvertedValues[1] != 0xFFFF) { printf(''%X %X \n'', ADCConvertedValues[0], ADCConvertedValues[1]); //ADCConvertedValues[1] = 0xFFFF; } } } static void ADC_Config(void) { ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; DMA_InitTypeDef DMA_InitStructure; /* Enable peripheral clocks *************************************************/ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3, ENABLE); /* DMA2_Stream0 channel0 configuration **************************************/ DMA_DeInit(DMA2_Stream0); DMA_InitStructure.DMA_Channel = DMA_Channel_2;// Channel 0 as mentionned in the datasheet ?? DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC3->DR;// Address of ADC3 peripheral ?? DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCConvertedValues[0];// pointer on my data DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;// From ADC to memory DMA_InitStructure.DMA_BufferSize = 3;// 2 data to bring back (2 ANA input) DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;// No incrementation of peripheral, always read at the same address DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA2_Stream0, &DMA_InitStructure); /* DMA2_Stream0 enable */ DMA_Cmd(DMA2_Stream0, ENABLE); /* ADC Common Init **********************************************************/ ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC3 Init ****************************************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_8b; ADC_InitStructure.ADC_ScanConvMode = ENABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge =ADC_ExternalTrigConvEdge_None ; ADC_InitStructure.ADC_ExternalTrigConv =ADC_ExternalTrigConv_T1_CC1 ; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 2; ADC_Init(ADC3, &ADC_InitStructure); /* ADC3 regular channel configuration ******************************/ ADC_RegularChannelConfig(ADC3, ADC_Channel_9, 1, ADC_SampleTime_480Cycles);//PF3 ADC_RegularChannelConfig(ADC3, ADC_Channel_14, 2, ADC_SampleTime_480Cycles);//PF4 /* Enable DMA request after last transfer (Single-ADC mode) */ ADC_DMARequestAfterLastTransferCmd(ADC3, ENABLE); ADC_DMACmd(ADC3, ENABLE); **************************************************************/ ADC_Cmd(ADC3, ENABLE); } #selective-cut-n-paste2014-01-13 7:25 AM
someone can help me, my code is:
Looks a bit familiar, but post ALL of it, I have better things to do than recreate the half that's missing.2014-01-16 12:46 AM
Yes i follow another example, but i' ve resolved i forget the GPIO configuration.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.