2014-01-16 12:04 AM
Nothing weird in the ISR.
I used a standard example, just added a few Pin toggles to follow with LEDs. Don't see it entering the ISR during DEBUG Mode at all though. - Got it - found the problem ! One of the mcp2551 chips (or both) is not working. So I use the Diode circuit below, and got rid of the failed mcp2551 chips. It enters into the ISR properly repeatedly on schedule now ! Data is not always perfect - but can solve that at my ease (via protocols). Learned Notes: 1) Connecting CAN Tx to Rx on same Chip - will Not work. It will just continuously Resend without Receiving in the ISR. If it answered its own message - how could any other Node/Chip answer it then ? 2) Connecting TxRx to another chip RxTx with common Gnd does not work. 3) Can use Simpler DIODE circuit instead of a CAN chip which works somewhat ok. Link (2) micros together via a wire connected to the CAN RX lines and Diodes connecting the TX (as a drain) to the same line. And, using a common Gnd wire. Micro1: Micro2: CAN RX <-------+-------------+-------> CAN RX | | CAN TX >--|<--+ +-->|--< CAN TX Gnd o-----------------------------------------o Gnd This gives a lot simpler setup for Debugging.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.