2015-02-02 10:19 AM
Is there a way to add the processor temperature, and battery voltage, internal ADC channels to the conversion list in CubeMX 4.6.0?
The interface doesn't seem to support it.2015-03-19 6:40 AM
Hello Andrei,
In general, if it is supported by the ADC instance, in the pinout tree you can see the dedicated mode for temperator sensor, VBAT and Vrefint Channels. (please refer to the attached screenshot). If it is not the case, could you please indicate the used mcu. With Best regards. ________________ Attachments : ADC1.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzRT&d=%2Fa%2F0X0000000bNO%2Fsg64DRH.NYHdycyKK8sX6Nz4pJCZ.F6cgM.2pdU3kx0&asPdf=false2015-03-19 9:02 AM
I found it on the ''Pinout'' tab, not exactly user obvious since those 3 channels can't be routed to a pin.
I'd expect it to be on the ''Configuration'' tab, but I suppose ST's user testing showed that the pinout tab was the place to put it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.