2021-02-22 4:05 PM
Hi,
Anyone here successfully connected STM32F103C8T6 clone board using ST-LINK V3SET ?
QUESTIONS:
1. Here is the pins connection layout using CN2 JTAG:
+5V external ----> T_VCC pin 1
GND ---------------> GND pin 20
SWDIO ------------> T_SWDIO pin 7
SWCLK ------------> T_SWCLK pin 9
The actual connection is like below:
STM32CubeProgrammer already upgraded to latest ST-LINK V3SET firmware V3.J7.M2.B4.S1,
but I am unable establish connection to the STM32F103C8T6 board as shown picture below and the STM32CubeProgrammer CANNOT BE CLOSED:
I have reset by pressing the RESET button ( Software/Hardware reset options selected ) then followed by clicking the Connect button, the result still the same as shown above, any idea ?
My new ordered Nucleo F103RB board is on its way, but now I just wanted to test the STM32F103C8T6 clone board which is very common.
Please advise if there is any error connection above, I am new to ST-LINK V3SET.
2. The ST-LINK V3SET COM LED from the datasheet is stated Red color on power on, but sometime I notice it auto turned to Green color, is this normal ?
3. The ST-LINK V3SET cannot works if connected to a USB HUB, I have to isolate it to connect to a standalone USB port, what's the reason ? ( this is not practical as I have to unplug and plug in back manually and easily can damage the USB socket/connector in long run, the PC is far away from my workbench desk, I purposely need to use a long USB female socket cable and if with USB HUB, I can easily turn the switch ON/OFF ).
Thank you.
2021-02-24 2:23 AM
The StlinkV3 is advertised as STM8 and STM32 tool, but not a general SWJ Adapter for all kinds of CPUs. So it is not a fault that it does not connect to other CPUs
2022-05-04 2:37 AM
I agree. Not working through a hub surely indicates that the ST-LINK is not USB compliant or so flaky is upset by the presence of one. It's a right pain on my setup which is a desktop on the floor.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.