2017-06-25 4:07 AM
When i want to produce a pwm complementary output ,the chip is stm32f103c8, only main connel have output and auxiliary have no output . I track program to file stm32f1xx_hal_tim.c on funtion : TIM_OC1_SetConfig and find line:
tmpccer &= ~TIM_CCER_CC1NE; This line is wrong and shoud be change to : tmpccer |= TIM_CCER_CC1NE;Other fucntion as to TIM_OC2_SetConfigTIM_OC3_SetConfig
,have same error.2017-11-24 12:35 PM
This did solve my problem but I think there is a little more to this.
After reading your post I looked at theTIM_OC_InitTypeDef structure within stm32f4xx_hal_tim.h and found the declaration:
typedef struct
{
uint32_t OCMode; /*!< Specifies the TIM mode.
This parameter can be a value of @ref TIM_Output_Compare_and_PWM_modes */
uint32_t Pulse; /*!< Specifies the pulse value to be loaded into the Capture Compare Register.
This parameter can be a number between Min_Data = 0x0000U and Max_Data = 0xFFFFU */
uint32_t OCPolarity; /*!< Specifies the output polarity.
This parameter can be a value of @ref TIM_Output_Compare_Polarity */
uint32_t OCNPolarity; /*!< Specifies the complementary output polarity.
This parameter can be a value of @ref TIM_Output_Compare_N_Polarity
@note This parameter is valid only for TIM1 and TIM8. */
uint32_t OCFastMode; /*!< Specifies the Fast mode state.
This parameter can be a value of @ref TIM_Output_Fast_State
@note This parameter is valid only in PWM1 and PWM2 mode. */
uint32_t OCIdleState; /*!< Specifies the TIM Output Compare pin state during Idle state.
This parameter can be a value of @ref TIM_Output_Compare_Idle_State
@note This parameter is valid only for TIM1 and TIM8. */
uint32_t OCNIdleState; /*!< Specifies the TIM Output Compare pin state during Idle state.
This parameter can be a value of @ref TIM_Output_Compare_N_Idle_State
@note This parameter is valid only for TIM1 and TIM8. */
} TIM_OC_InitTypeDef;�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
It looks fine but when I looked at older version of similar code I found that the
TIM_OCInitTypeDef, which is the predecessor of
TIM_OC_InitTypeDef, it used to have these two members:
TIM_OutputState
TIM_OutputNStateThese two members configured the output state. The line you are referring to inside the
stm32f1xx_hal_tim.c (in my case stm32f4xx_hal_tim.c) follows a similar pattern to how the timer is initialized. First, the configuration bit in question is clearedand then configured with the appropriate using a member of the
TIM_OC_InitTypeDef structure
. Unfortunately, this 'output state' was not included in the new version of the structure and that bit was never enabled.I do agree with you that there is no way, that I see, that the complementaryPWM output bit can be enabled. with the code the way it is.
https://community.st.com/people/dengrui.dengrui
Serious kudos to you, thanks for the catch! I've spent more than 4 hours wondering what was wrong with my code and test equipment.Dave
2017-11-26 9:54 AM
Okay, I was wrong, I found there is a function called HAL_TIMEx_PWM_Start_IT Will do the same things as both dengrui dengrui and I did.
As an example, in order to start the complementary channel on channel 1 of timer 1 then the call looks like this:
HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_1);�?�?�?�?�?�?
Dave
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.