2022-02-16 6:39 AM
I am interfacing a 5V PWM signal with an STM32F030K6T6 MCU using PB0. According to the datasheet this pin is 5V Tolerant. In the past, regardless of a pin's "tolerance" to 5V I have always used a level shifter to change this 5V signal to a 3.3V signal before it gets to the MCU; "Just to be safe". This application I am trying to limit the number of parts on the PCB for both size and cost reasons. Testing on a Nucleo board seems to work and the MCU seems to tolerate this well, but for long term use in the field is it better to run this signal through a level shifter or does it not matter since the pin is "5V Tolerant"?
Solved! Go to Solution.
2023-12-15 8:23 PM
> It may seem redundant - but to confirm can we interface a 5V UART Input signal to the UART Rx pin which is 5V tolerant ie FT?
Yes, if the chip is powered prior to receiving a 5V signal, as stated above.
2025-02-05 9:24 AM
Hi, I am using a STM32H753ZI MCU and have configured an FT pin (PC0) for 5V digital inputs. However, since the pin is floating I have enabled the internal pull-down resister via CubeIDE. While testing it worked fine, but is there any damage this could cause to the board in the long run?
Thanks
2025-02-05 11:35 PM
You don't need to ask your question twice - see the answer here.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.