2012-09-18 12:16 AM
Hi everybody. I'm trying to display a bmp on 3,2'' TFT by using FSMC and stm32f4 graphic drivers. I've done writing some texts changing backcolour drawing pixels but when I want to draw or drive a bmp file with LCD_DrawMonoBMP or LCD_DrawColorBMP functions LCD shows me just white with some noisy white image. I added the screenshot. I need some help. Thanks a lot..
2012-09-28 12:48 AM
There is no issue now thank you but I did not see printf output window. are those hardfault_handler asm codes solving the problem automatically?
2012-09-28 2:22 AM
... are those hardfault_handler asm codes solving the problem automatically?
Certainly not. It is assumed to provide more information about the problem that caused the hard fault. I would be cautious with using printf() calls from inside the HardFault_Handler. Depending on the implementation, this might invoke a longer chain of function calls, which rely on things that your hard fault might have destroyed. I would rather set a breakpoint into the handler, and step through to check what happened and gather information about the hard fault.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.