STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Starting with STM32

Posted on September 24, 2012 at 15:46Hi, I'm migrating from 8-bit AVR to STM32. I have purchased already a STM3220G-EVAL board with STM32F207 CPU. The first task I want to accomplish is to get a ''Hello World'' application running on this board via ...

dimax by Senior
  • 4003 Views
  • 14 replies
  • 0 kudos

SMT32F103x_XL FLASH bank 2 stays BUSY

Posted on September 12, 2012 at 08:21Hi all,I am using an STM32F103ZG with the STM32F10x_StdPeriph Library. I started the development of the project with Keil ARM-MDK but now moved over to GCC.The switch over has gone pretty smooth until now. I use ...

hermanv by Associate II
  • 1501 Views
  • 1 replies
  • 0 kudos

3,2'' TFT LCD with FSMC

Posted on September 18, 2012 at 09:16Hi everybody. I'm trying to display a bmp on 3,2'' TFT by using FSMC and stm32f4 graphic drivers. I've done writing some texts changing backcolour drawing pixels but when I want to draw or drive a bmp file with L...

0690X00000602lYQAQ.jpg

STM32F405: Read 100% duty cycle

Posted on September 27, 2012 at 11:21I am using STM32F405 in an application and in order to start working with the PWM module I have to check that I read a 100% duty cycle on one channel input. I've been reading documentation, but it seems that inp...

miriarte by Associate II
  • 2642 Views
  • 6 replies
  • 0 kudos

maximum throughput for usart

Posted on September 25, 2012 at 04:22Hello All,   Finally got to a stm32 discovery specific question. I've turned my baud up to a really high rate 921600. I have a simple loop that sends a request for data and then gets data back from the stm32 as f...

Checking for USART Buffer Overflows

Posted on September 27, 2012 at 15:27Should I be checking for buffer overflows? Do I just clear the bit if the interrupt occurs? What is the best way to handle buffer overflows?

wbarkley by Associate II
  • 2285 Views
  • 5 replies
  • 0 kudos

Help getting started with FatFS please (SPI bus, STM32F4)

Posted on September 20, 2012 at 16:53I've recently switched to using an ST microcontroller and am in need of some assistance getting FatFS to work. I've never worked with FatFS before but it seems to be the go-to module for implementing the Fat file...

kwheaton by Associate II
  • 5362 Views
  • 16 replies
  • 0 kudos

stm32F205: 96 unique ID: use only 32

Posted on September 27, 2012 at 18:35Does anybody know if the 96bit unique-ID has different fields? There's no much info about this unique ID (in the reference manual it is said that it has 96bits but after that, when the register is shown only the ...

miriarte by Associate II
  • 1842 Views
  • 1 replies
  • 0 kudos

Break / PWM - STM32F4

Posted on September 27, 2012 at 10:41Hi Folks, I like to disable PWM, on an external event - i want to use BKIN. i set the break mechanism up like this ------......    GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_TIM1);     /* Automatic Output ...

finnb2 by Associate II
  • 1570 Views
  • 3 replies
  • 0 kudos

Break / PWM - STM32F4

Posted on September 27, 2012 at 10:30Hi Folks, I like to disable PWM, on an external event - i want to use BKIN. i set the break mechanism up like this ------......    GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_TIM1);     /* Automatic Output ...

finnb2 by Associate II
  • 1425 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.