2019-05-08 3:11 AM
We have STM3240G-Eval and STEVAL-IHM028V2 boards.
we are trying to run the bldc motor of (24 pole-pairs,1.4KW) with motor profiler (MC-SDK 5.3.3) and we also tried with another motor (8 pole-pairs , 30W) .
the profiler isn't able to calculate Rs, Ls and Ke Values. but after 20% to 25% of profiling it is showing "The measurement is talking too much time".
we also decrease current and max. speed but the result are same.
2021-06-14 11:49 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.