2020-09-16 3:17 AM
I have a drone bad behavior when i request opposite large stick movement. I think i need to set a ramp to have homogenous movement . For little stick movement there is normal reaction then i stabilize it easily but when i need to inverse the command with a large stick movement example before i reach a wall, there is over reaction. I would like to set a ramp near the ramp value when hDurationms = 0
Solved! Go to Solution.
2020-09-16 8:33 AM
"I have a drone bad behavior when i request opposite large stick movement" have you tried Tuning the PIDs? There are 2 reasons why you aren't achieving instantaneous fast speeds: 1) the motor is not able to achieve that 2) PIDs needs tuning (try increasing KP or decrease kd of the speed PID regulator) . At least this was the case for me.
2020-09-16 8:33 AM
"I have a drone bad behavior when i request opposite large stick movement" have you tried Tuning the PIDs? There are 2 reasons why you aren't achieving instantaneous fast speeds: 1) the motor is not able to achieve that 2) PIDs needs tuning (try increasing KP or decrease kd of the speed PID regulator) . At least this was the case for me.
2020-10-01 1:06 AM
Dear @richard orengo
Does the @msingh's answer solve your problem?
Best regards
Laurent Ca...
2020-10-01 6:22 AM
hello,
yes. I have successfully tuned PID, thx
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.