2024-02-14 5:44 AM - edited 2024-02-14 5:47 AM
MCSDK 6.2.0 introduced erronous conversions from float_t to int16_t in:
The bug persist in MCSDK 6.2.1.
MCI_ExecTorqueRamp_F is implemented mc_interface.c.ftl
/**
* @brief Programs a motor torque ramp
*
* pHandle Pointer on the component instance to work on.
* FinalTorque is the value of motor torque reference at the end of
* the ramp. This value represents actually the $I_q$ current expressed in
* Ampere.
* Here the formula for conversion from current in Ampere to digit:
* I(s16) = [i(Amp) * 65536 * Rshunt * Aop] / Vdd_micro.
* hDurationms the duration of the ramp expressed in milliseconds. It
* is possible to set 0 to perform an instantaneous change in the
* value.
*
* This command is executed immediately if the target motor's state machine is in
* the #RUN state. Otherwise, it is buffered and its execution is delayed until This
* state is reached.
*
* Users can check the status of the command by calling the MCI_IsCommandAcknowledged()
* function.
*
* MCI_ExecTorqueRamp
*/
__weak void MCI_ExecTorqueRamp_F(MCI_Handle_t *pHandle, const float_t FinalTorque, uint16_t hDurationms)
{
#ifdef NULL_PTR_CHECK_MC_INT
if (MC_NULL == pHandle)
{
/* Nothing to do */
}
else
{
#endif
int16_t hFinalTorque = ((int16_t)FinalTorque * (int16_t)CURRENT_CONV_FACTOR);
MCI_ExecTorqueRamp(pHandle, hFinalTorque, hDurationms);
#ifdef NULL_PTR_CHECK_MC_INT
}
#endif
}
The conversion on line 33 truncates FinalTorque before scaling to the internal representation. This means that a ramp to e.g. 1.7A will actually only execute a 1.0A ramp.
In MCSDK 6.1.2, the conversion was handled correctly.
int16_t hFinalTorque = (int16_t) (FinalTorque * CURRENT_CONV_FACTOR);
Similar wrong conversions has been introduced to MCI_ExecSpeedRamp_F and MCI_SetCurrentReferences_F.
I suspect that the bug was introduces when fixing a bug in the opposite conversions in functions such as MCI_GetLasRampFinalSpeed_F.
// Wrong conversion in MCSDK 6.1.2
RetVal = (float)((pHandle->hFinalSpeed * U_RPM) / SPEED_UNIT);
// Correct conversion in MCSDK 6.2.0
reVal = (((float_t)pHandle->hFinalSpeed * (float_t)U_RPM) / (float_t)SPEED_UNIT);
Solved! Go to Solution.
2024-02-14 6:49 AM
Hello,
Thank you very much for your bug report.
I will enter a ticket on our side, and it will be solved on further version.
2024-02-14 6:49 AM
Hello,
Thank you very much for your bug report.
I will enter a ticket on our side, and it will be solved on further version.
2024-05-17 1:23 AM
Hello,
This issue has been fixed in our new MCSDK 6.3.0 release,
so feel free to download it and try if it solved correctly your issue reported in this post.
Kind Regards.
Amina.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.