STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Problem with encoders on Nucleo-446RE.

Hello!Im working at inspecting vechicle. It is made of nucleo-446re, DRV8835 motor driver, two DC motors and two optical encoders mounted on motros. The encoders are manufactured by Pololu. First encoder is conected to TIM3 CH1 and CH2 on pins PA6 an...

KWikt.1 by Associate
  • 1396 Views
  • 2 replies
  • 0 kudos

Using ICS

Dear HelpersI can run a motor with three shunt resistors. Now I tried to use ICS. Firmware was downloaded to STM32F103RC with no error. But when I started to run the motor, Workbench indicated "Unknown" fault. Stop button was clicked it became "Any S...

SWoo.1 by Associate
  • 1343 Views
  • 2 replies
  • 0 kudos

Resolved! L6470 NEMA17 MotorParameterData_t for 10rps (2000 steps/s)

Hi All, I'm using ​NUCLEO-F401RE + X-NUCLEO-IHM02A1 + NEMA17 stepper motor. Motor stalls above 6rps (1200steps/sec). Can someone share MotorParameterData_t for  NEMA17 stepper motor, 103H5210-5240 (SANYO DENKI - SANMOTION 103H5210-5240 Stepper Motor)...

S.Kamath by Associate III
  • 3260 Views
  • 10 replies
  • 0 kudos

Resolved! Can't find STEVAL-SPIN3204 in Motor Control Workbench 5.4.4

Hi everyone:I had bought a STEVAL-SPIN3204 for my BLDC motor project. There are two question I want to ask.1. I can't find STEVAL-SPIN3204 in Motor Control Workbench 5.4.4 list. 2. I can't find STSPIN32F0B in MCU list.Does anyone meet the same proble...

0693W000004GfC6QAK.jpg 0693W000004GfBmQAK.jpg
YLiu.4 by Associate
  • 1336 Views
  • 2 replies
  • 0 kudos

Motor profiler and MX generated code not working properly

Hy all,I have a little problem. I am using a B-G431b-ESC1 developement kit. I generated a code with the help of Motor control Workbench and MX. I followed the steps from:https://www.st.com/content/ccc/resource/technical/document/user_manual/group1/...

N_1 by Associate II
  • 1627 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.