2022-01-11 8:59 AM
I'm using MotorControl Workbench 5.Y.3 + Keil MDK
Testing on EVSPIN32G4 and custom STSPIN32G4
54V battery, 16A nom current
2022-01-12 6:26 AM
Perhaps your question is related to my question. And I have the same problem.
I think about the fact that the FOC algorithm cannot correctly start the rotation of the motor under a heavy load and this requires trapezoidal control at the first moment. I would be just as interested to know ST's answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.