STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! can FOC Frequency be very low?

I've designed an FOC board.First of all,I want to realize the SVPWM without using other transformation in order to make the motor rotate first.PWMC_SetPhaseVoltage(pwmcHandle, Valphabeta);so I generate an array about Valphabeta as the code below:#de...

Lzhiy.1 by Associate II
  • 1718 Views
  • 2 replies
  • 0 kudos

issue on ADC sampling point

in fuction:uint16_t R3_2_SetADCSampPointSectX( PWMC_Handle_t * pHdl ) /* sector number needed by GetPhaseCurrent, phase A and B are sampled which corresponds * to sector 4 */ pHandle->_Super.Sector = SECTOR_4;Phase A and B is corresponding t...

0693W00000GY7lVQAT.jpg
Lzhiy.1 by Associate II
  • 1520 Views
  • 1 replies
  • 1 kudos

Resolved! (Environment: MCSDK 5.Y.2 + STM32CubeMX 6.3.0) NUCLEO-F446RE is not working compared to other NUCLEO boards while using the same power board & BLDC motor with the same configuration. What would be the possible cause for this problem?

(Environment)MCSDK 5.Y.2, MC Workbench 5.Y.2, CubeMX 6.3.0​, IAR EWARM 8.50(Test Result)NUCLEO-G431RB + X-NUCLEO-IHM16M1 + GBM2804H-100T(BLDC sensorless) => working wellNUCLEO-L476RG + the same board & motor & configuration => working wellNUCLEO-F446...

0693W00000GWjNhQAL.jpg 0693W00000GWjNmQAL.png
THA.1 by Associate II
  • 4806 Views
  • 9 replies
  • 0 kudos

Resolved! Help on regenerative Braking for electric vehicles.

I am really struggling hard to understand the regenerative braking for electric vehicles for 48V systems. My main doubt is if the motor back emf is less than battery voltage, how does it do generation. The motor is PMSM with sinusoidal back emf and i...

VD.3 by Associate II
  • 2921 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.