2018-09-21 5:51 AM
I generate a STEVAL-SPIN3202 project (Keil MDK) by ST Motor Control Workbench V5.2. But it doesn't work. The motor was BR2804-1700kv-1 sensor less motor from P-NUCLEO-IHM001 KIT.
Motor didn't really spin. I got FOC duration faults when I started motor in Monitor page of Motor Workbench. Communication was OK without problem.
I have other two ST evaluation KIT which are P-NUCLEO-IHM001 and STEVAL-ESC001V1. Both of them work perfectly with ST Motor Control Workbench V5.2 and BR2804-1700kv-1.
My questions are:
Thanks,
Ian
2021-06-22 2:15 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.