STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

STEVAL-SPIN3201 randomly disconnects

Posted on May 26, 2017 at 16:09Working with STEVAL-SPIN3201. The board seems to randomly disconnect. It is not related to running a motor, just connected to motor control workbench. SPIN32F0 drive stays enumerated under windows. Anybody seen this?

USART not working in Motor Control Library

Posted on July 14, 2017 at 15:32I am using the Motor Control Library, to control a BLDC motor with Hall sensors. I would like to use the uart for my own purposes. If I enable uart, it dumps trash (since it tries to communicate with the MC workbench)...

About MotorProfiler motor data

Posted on July 18, 2017 at 05:36HiI'm working with the MotorProfiler to create the motor id data.But I create too much motor id data, so the motor control Workbench is a mess, as picture below.How can I delete some motor id data?Regards,Hank

0690X00000607IbQAI.png
Hank Wu by Associate
  • 939 Views
  • 1 replies
  • 0 kudos

LA052-080E3NL1 Shinano motor: how can I purchase it

Posted on July 28, 2017 at 14:43Hello,I would like to purchase 1 unit of LA052-080E3NL1 Shinano motor to be able to evaluate one of the reference project of the motor control workbench: How can I purchase it?Thank you.#motor #la052-080 #shinano #mot...

ST Motor Control Workbench: How to let the ''Enable differential term'' checkbox in ''Speed regulator'' be valid?

Posted on August 14, 2017 at 07:13I am using ST Motor Control Workbench and want to add differential term in the speed regulation of motor. But the checkbox 'Enable differential term' in 'Drive Management->Drive Settings->Speed Regulotor' is always ...

X TY by Associate
  • 1076 Views
  • 1 replies
  • 0 kudos

PFC doesn't work on STEVAL-IHM034V2 board

Posted on August 25, 2017 at 11:12Hi,i'm using the a STEVAL-IHM034V2 board for evaluation (PFC + FOC PMSM).I imported the project in ST Workbench 4.3. Generated files and compiled with IAR is OK. Then board is programmed.The motor starts but the PFC...

''Connection Failed!'' to STEVAL-SPIN3201

Posted on October 24, 2017 at 09:32Hi Community, I'm trying to talk to to STEVAL-SPIN3201 within the Monitor of ST Motor Control Workbench (v.4.3), running on a Microsoft Surface Pro 2 Windows 8, connected by USB (COM3 at 9600 baud), but I keep gett...

STM workbench failed to connect control board

Posted on November 11, 2017 at 09:01Software: ST Motor Control Workbench V4.3.0.16508MCU: STM32F051C6T6Phenomenon:  use serial port connect to MCU always fail. Some times can connect to MCU, but lose connection soon: Error msg: 'Communication is clo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.