2024-08-22 9:51 AM - edited 2024-08-22 9:53 AM
Hi,
I've been using my custom board with the STM32C011G6 MCU as a control board. By customizing the JSON file on the power board, I've been able to generate a project through MC Workbench -> CubeMX -> CubeIDE, and the motor driver has been running well. However, a new revision of the custom board requires me to reroute my UART pins to PA9 and PA10. Since the STM32C011G6 doesn't have standalone PA9 and PA10, I need to remap PA11/PA12 to PA9/PA10. Unfortunately, I don't see this feature in MC Workbench. Directly assigning PA9/PA10 in the JSON file results in the GUI indicating that the UART feature is not supported. How can I resolve this?
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.