2021-06-23 11:44 AM
Hi.
I'm trying to spin my motor using ST Motor Control WB and STM32CubeIDE. In my code I programmed motor speed 1500rpm, but instead of that my motor started to spin with 9000rpm speed. When I set 6500 or 9000rpm speed it spins with 1800rpm. If I try to set it using Motor Control WB or Motor Pilot is spins correctly. Can someone help me with my code in IDE?
2021-06-27 7:43 PM
Dear @Kamil Wroński
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.