2024-05-17 1:24 AM
[VERSION]: 6.2.1
[TOOL]: Motor Profiler in Motor Pilot V1.2.5
[DETAILS]:Motor Profiler gets stuck while profiling at "Profiling % 28".
Hardware used is the inverter-board B-G431B-ESC1.
[EXPECTED BEHAVIOR]: I expect the motor profiler to either finish the process or abort with an error so that I can fix any existing issues.
[HOW TO REPRODUCE]: Motor is soldered to the inverter-board, power supply connected and set up to deliver the correct voltage and enough current (12V, 30A). Motor Profiler is started and connects successfully. The required motor parameters are entered accordingly. The profiling is started. At 7%, the motor twitches once, and at 21% the motor hums for half a second. Maximum observed current is around 2.5A until then. Then the process gets stuck at 28% until the notification pops up that the measurement takes too long. The board pulls standby current.
2024-12-02 7:15 AM
How would I go about doing that?
2024-12-02 7:38 AM
Hello DMeie.2,
Well, I explained it a bit in my previous answer, but you can get help from the Open Loop documentation in the User Manual.
2024-12-03 1:44 AM
I already have set a known working Start-up profile for the motor into the Profiler project.
As for Open-Loop mode, I have used this before.
However, I am not sure how to enter these values into the Profiler project, as it is not possible to have Profiler and Open-Loop mode at the same time.
2025-10-20 7:38 AM
I have the same problem. I connected a PMSM motor, but it gets stuck at 28%. I tried changing the maximum current and maximum RPM, but it didn’t work. I also tried running it in open-loop mode, but as soon as I start, it shows an “Error Over.” What should I do?
I tested with an AC induction motor in open-loop voltage mode, and it works fine. However, when I switch to the PMSM motor, it doesn’t work.
2026-02-11 4:44 AM - edited 2026-02-11 4:46 AM
Hi all,
I would like to follow up on this post, as I am experiencing the same issues.
Motor: Faulhaber 0620B
Nucleo: F446RE
Driver: IHM17M1
MCSDK: V6.4.1
I was easily able to spin the motor up in open loop mode to a whole range of speeds at a wide range of currents.
However, when I run the profiler, the motor spins up and then fails about halfway to the target speed. The profiler then hangs at 28%.The speed up seems perfectly fine, and I have tried both with aux hall sensors and without. I have also tried a wide range of speeds from 50000RPM to 5000RPM, and all currents from 0.1-0.3A.
Any help would be appreciated.
Kind regards,
J Frey
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.