STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Motor Profiler stuck at 28%

[VERSION]: 6.2.1[TOOL]: Motor Profiler in Motor Pilot V1.2.5[DETAILS]:Motor Profiler gets stuck while profiling at "Profiling % 28".Hardware used is the inverter-board B-G431B-ESC1.[EXPECTED BEHAVIOR]: I expect the motor profiler to either finish the...

DMeie.2 by Senior II
  • 6222 Views
  • 14 replies
  • 1 kudos

Max speed of the motor not achieved

Hardware Details: Custom Hardware based on the B-G431B-ESC1, 3 phase, Hall sensored FOC,MCSDK: 6.4.1The maximum speed of the motor is 3000 RPM. I have run the motor using motor profiler software and the profiler shows the maximum speed is 2500, Rs = ...

STuser2 by Senior III
  • 275 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.