2025-12-16 12:32 AM
Hello ST Team,
I am working with the B-G431B-ESC1 board using STM32G431CBU6 and the STM32 Motor Control SDK.
On the evaluation board, Motor Pilot communicates with the target MCU through the on-board ST-LINK (STM32F103) using SWD and VCP.
My question is:
Is it possible to use STM Motor Pilot to communicate directly over UART with the STM32G431 (for example via an external USB-to-TTL adapter), without using the on-board or external ST-LINK?
2025-12-16 7:59 AM
It will work i am not sure what is the confusion. You can refer the below start up guide
STM32 MC Motor Pilot - Start-up guide - stm32mcu
You have to use the USB to TTL adapter, i am just referring the serial part number you can use to connect to motor pilot. FT232RL USB to TTL Serial Adapter Module 5V/3.3V
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.