2024-06-12 4:24 AM
Hey everyone!
I was just exploring different features of the ST MCSDK and encountered the on-the-fly startup option dedicated to fan application.
Whenever I check this option, after the startup procedure, the motor accelerates to its nominal speed and then the firmware somehow takes control and run the closed loop to control the speed.
I tried to eliminate this behavior and changed a lot of parameters including speed PI coefficients and it didn't work
Is this behavior normal or am I missing something?
Has anyone had the same problem? Could you please guide me if you have any idea?
Thanks a lot!
Solved! Go to Solution.
2024-06-15 3:04 AM
Hey everyone,
to achieve this purpose, We need to check the Rev-UP algorithm in order to have a smooth transition between the open loop and the closed loop sensorless algorithm.(See what I have attached)
Having done that, I observed that there was no peak in the speed after switching to the closed loop
Try this because it may help!
Regards.
2024-06-15 3:04 AM
Hey everyone,
to achieve this purpose, We need to check the Rev-UP algorithm in order to have a smooth transition between the open loop and the closed loop sensorless algorithm.(See what I have attached)
Having done that, I observed that there was no peak in the speed after switching to the closed loop
Try this because it may help!
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.