STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Resolved! User button use

How to use in main.c the user button of B-G431B-ESC1 board ?I want to togle the position each time I press (amd release) the button.Waiting for target position completed and than I can press the button again.I have selected the PC10 pin in MXCube tha...

UniRob by Associate III
  • 2449 Views
  • 2 replies
  • 0 kudos

STSPIN32G4 standby mode issue

I am testing the Standby mode with the EVSPIN32G4 board. However, it is not entering standby mode. When I check the Vcc voltage, it outputs 8V despite being set to standby mode. Have you checked if a functional test for standby mode has been conducte...

secupol by Associate
  • 1049 Views
  • 0 replies
  • 0 kudos

Resolved! Stm32G431B-ESC-1 motor direction with pwm

Hi, I have managed to get my ipm motor running with hall sensors. I can run the motor with motor pilot no problem. I can run the motor down to zero rpm and in reverse direction. I have it running with a pwm signal generated on an arduino in forward r...

TRowe by Associate II
  • 3974 Views
  • 4 replies
  • 1 kudos

Bug: RTOS task scheduler too fast

MCWB Version: 6.2.1CubeMX Version: 6.10.0Issue: I generate a default project for the B-G431-ESC1. Only settings I change is to enable the FreeRTOS with TIM6 as the tick timer. Firmware Package Version is V1.5.1 (Recommended).Via CubeMX I add a GPIO o...

DMeie.2 by Senior II
  • 5176 Views
  • 8 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.