2026-01-10 5:49 AM - edited 2026-01-10 5:53 AM
Hi,
I wonder how the motor control unit should behave if a speed ramp is programmed right after a torque ramp?
Following code snippet shows this setup:
// Set Torque/Iq limit
MC_ProgramTorqueRampMotor1(iqLimit, 0);
// Programm speed ramp
MC_ProgramSpeedRampMotor1(speed, 500);
// Start motor
MC_StartMotor1();Do I understand correctly that this code should lead to the following behavior?
the motor starts in speed mode
if the load driven by the motor increases the speed will decrease
if the load increases further the motor will run with decreasing speed until it reaches the torque/iq limit set by the MC_ProgramTorqueRampMotor1() function
the motor will stop and deliver a constant torque - the torque programmed with MC_ProgramTorqueRampMotor1()
Best regards
B0bbyR4y
Solved! Go to Solution.
2026-01-10 8:24 AM
If one command execution is in progress it will not execute the next command. Refer the below documentation in the code
/**
* @brief Returns information about the state of the last buffered command.
* @PAram pHandle Pointer on the component instance to work on.
* @retval The state of the last buffered command
*
* The state returned by this function can be one of the following codes:
* - #MCI_BUFFER_EMPTY if no buffered command has been called.
* - #MCI_COMMAND_NOT_ALREADY_EXECUTED if the buffered command
* condition has not already occurred.
* - #MCI_COMMAND_EXECUTED_SUCCESSFULLY if the buffered command has
* been executed successfully. In this case calling this function resets
* the command state to #MCI_BUFFER_EMPTY.
* - #MCI_COMMAND_EXECUTED_UNSUCCESSFULLY if the buffered command has
* been executed unsuccessfully. In this case calling this function
* resets the command state to #MCI_BUFFER_EMPTY.
*/
__weak MCI_CommandState_t MCI_IsCommandAcknowledged(MCI_Handle_t *pHandle)This function is in the mc_interface.c file
and also refer
/**
* @brief Programs a torque ramp for Motor 1 for later or immediate execution.
*
* A torque ramp is a linear change from the current torque reference to the @p hFinalTorque
* target torque reference in the given @p hDurationms time.
*
* Invoking the MC_ProgramTorqueRampMotor1() function programs a new torque ramp
* with the provided parameters. The programmed ramp is executed immediately if
* Motor 1's state machine is in the #RUN states. Otherwise, the ramp is buffered
* and will be executed when the state machine reaches any of the aforementioned state.
*
* The Application can check the status of the command with the MC_GetCommandStateMotor1()
* to know whether the last command was executed immediately or not.
*
* Only one command can be buffered at any given time. If another ramp - whether a
* torque or a speed one - or if another buffered command is programmed before the
* current one has completed, the latter replaces the former.in mc_api.c file.
2026-01-10 8:24 AM
If one command execution is in progress it will not execute the next command. Refer the below documentation in the code
/**
* @brief Returns information about the state of the last buffered command.
* @PAram pHandle Pointer on the component instance to work on.
* @retval The state of the last buffered command
*
* The state returned by this function can be one of the following codes:
* - #MCI_BUFFER_EMPTY if no buffered command has been called.
* - #MCI_COMMAND_NOT_ALREADY_EXECUTED if the buffered command
* condition has not already occurred.
* - #MCI_COMMAND_EXECUTED_SUCCESSFULLY if the buffered command has
* been executed successfully. In this case calling this function resets
* the command state to #MCI_BUFFER_EMPTY.
* - #MCI_COMMAND_EXECUTED_UNSUCCESSFULLY if the buffered command has
* been executed unsuccessfully. In this case calling this function
* resets the command state to #MCI_BUFFER_EMPTY.
*/
__weak MCI_CommandState_t MCI_IsCommandAcknowledged(MCI_Handle_t *pHandle)This function is in the mc_interface.c file
and also refer
/**
* @brief Programs a torque ramp for Motor 1 for later or immediate execution.
*
* A torque ramp is a linear change from the current torque reference to the @p hFinalTorque
* target torque reference in the given @p hDurationms time.
*
* Invoking the MC_ProgramTorqueRampMotor1() function programs a new torque ramp
* with the provided parameters. The programmed ramp is executed immediately if
* Motor 1's state machine is in the #RUN states. Otherwise, the ramp is buffered
* and will be executed when the state machine reaches any of the aforementioned state.
*
* The Application can check the status of the command with the MC_GetCommandStateMotor1()
* to know whether the last command was executed immediately or not.
*
* Only one command can be buffered at any given time. If another ramp - whether a
* torque or a speed one - or if another buffered command is programmed before the
* current one has completed, the latter replaces the former.in mc_api.c file.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.