2021-10-17 2:24 AM
I started getting these errors on loading the ST Motor Pilot App (V0.9.9)
[WARNING] - MotorControlRegistersBank: Accessing register [977] STOCORDIC_C1 for motor 0 resulted in error[5] . Changing register's access accordingly to avoid getting this error again
[WARNING] - MotorControlRegistersBank: Accessing register [1041] STOCORDIC_C2 for motor 0 resulted in error[5] . Changing register's access accordingly to avoid getting this error again
[WARNING] - MotorControlRegistersBank: Accessing register [1680] DAC_OUT2 for motor 0 resulted in error[5] . Changing register's access accordingly to avoid getting this error again
[WARNING] - MotorControlRegistersBank: Accessing register [1616] DAC_OUT1 for motor 0 resulted in error[5] . Changing register's access accordingly to avoid getting this error again
How can I troubleshoot this?
2021-10-18 1:03 AM
Hello @GHave.1 ,
These lines are not errors but warnings.
It just means that the motor Pilot try to access non existant registers. This probably comes from your project configuration, if the DAC is disabled, then the code related to the DAC is not present in the firmware.
Note that with the release 5.Y.3 you have access now to the same signals through the motor Pilot than with the DAC.
Regards
Cedric
2021-10-28 10:01 PM
Thanks for the info. And I get that these are warnings, but I don't have any of that configured and I wasn't getting those messages - and then I was, and I don't know what triggered it. I guess, as long as operation isn't affected, it's ok, but the messages are annoying. If you know what to look for that I might have to go reconfigure, to get rid of them, I'd appreciate it.
Thanks.
2021-11-12 8:07 AM
Hello @GHave.1 ,
To remove the DAC warning, you can configure the DAC with the workbench. In the main window, you have a green box called "DAC Functionality" if you select Debug instead of "Not used" it will generate the registers accordingly, and will not dumped the warnings related to the DAC.
For other registers, we need to improve the Pilot to first read the configuration and after dump only registers available. This in in our todo list.
Regards
Cedric
2021-11-13 8:25 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.