2026-02-16 9:42 PM - edited 2026-02-16 9:43 PM
Hi,
I am working in steval-esc001v1. I have set the a2212-13t-1000kv bldc motor to ran at minimum of 1000 rpm and at maximum of 9924 rpm using the foc algorithm in the motor control workbench software. I have ran till the 8000 rpm. But our goal is to ran any type of motor with in the ESC's voltage rating of 3S to 6S (11 V to 22V), also Is it possible to calibrate esc by giving maximum pwm input and minimum pwm input without profiling the esc using pc software every time if the motor changes? If not possible, how does the general ESCs available in the market can do that. If anyone worked in these area, kindly assist.
Thanks and Regards,
Santhosh.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.