2021-07-06 5:18 PM
How can we determine if the computational power of only one STM32F103RB MCU is sufficient for controlling two BLDC motors? System clock is 72 MHz. For my current application I believe it is feasible due to low motor velocities, here up to 5 rev/sec per motor. However, is a good estimation technique available? Motor commutation will be based on Hall signals only (no field-oriented control, FOC). The Hall signals will be captured using the advanced timers 1 and 8.
2021-07-06 8:17 PM
Dear @Kmax18
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools or what version of those tolls you use (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
2021-07-06 9:51 PM
Hello Laurent, thank you for your response. I will provide more details in soon.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.