2025-10-23
2:23 AM
- last edited on
2025-10-28
12:49 AM
by
Maxime_MARCHETT
I am currently seeking to implement motor rotation control to any desired angle using the P-NUCLEO-IHM001 motor kit. Is this feasible? If so, how should I proceed? Are there any relevant tutorials or documentation available? Thank you.
*This post has been translated from Chinese to comply with the ST Community guidelines.
2025-10-23 6:59 AM
Hello @Lzj111111,
The language of the Community is English as mentioned here.
For motor position control, you need a motor with a quadrature encoder sensor. Refer to Position Control Application note for more details.
2025-10-26
8:40 PM
- last edited on
2025-10-28
12:49 AM
by
Maxime_MARCHETT
I have consulted the position control application notes and proceeded with configuration according to the documentation. However, regarding Figures 10 and 12 in the documentation, where exactly should I make the configurations as illustrated? Thank you.
*This post has been translated from Chinese to comply with the ST Community guidelines.
2025-10-28 2:26 AM
Hello @Lzj111111,
The mentioned application note corresponds to MCSDK5.x version; however, the API usage and PID tuning chapters remain valid.
For the MCSDK6.x version, refer to the Position Control link in the User Manual documentation available through Workbench tool > About > Documentations > Documentation, User Manual tab.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.