2021-12-09 9:29 AM
What I need to do is implement a command line interface over that serial port for factory configuration and settings controls. When I add printf() calls to the while loop in main I don't see my messages on the virtual COM port of my Discovery board. In my final board there won't be an embedded ST-Link so I will be using the physical serial port.
2021-12-09 9:38 AM
If the printf() isn't working you'll need to go over the plumbing, and how the _write() function uses __io_putchar(), and with which UART.
Perhaps get some static analysis tools and walk the code, understand the current topology and how that functions, and then integrate the functionality you want.
2021-12-09 1:14 PM
Don't I need to remove the code that is implementing the motor control protocol first? The UART works because I can use the MC Pilot program to connect to the board but I want that to not work so I can take over the UART for my purposes. I can do that but I was hoping that I wasn't the first to need to do this and there was a path I can follow that would be faster.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.