STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

I tried with Motor Control(X NUCLEO IMH 07M1 & NUCLEO F302R8 with ST BLDC Kit DONGXING WEI A2304-1700 ) workbench with some default examples for FOC speed control but the result was not promising. No movement is happening to motor can u help me in same?

I am test the motor in motor profiler with Jumper settingsIn NUCLEO F302R8 Jumper JP5 is in E5V : External voltage is planned to supply using a 12 V adapter to X NUCLEO IMH 07M1 boardJ7 DAC/REF in X NUCLEO IMH 07M1 is kept open J7 DAC/REF in X NUCLEO...

GSrik.2 by Associate
  • 1624 Views
  • 2 replies
  • 0 kudos

Resolved! BR2804 motor 1700kv-1, parameters or datasheet. I am using P-NUNCLEO-IHM001 package(nucleo-F302R8, STSPIN L6230 motor driver, BR2804 motor 1700kv-1) to performance FOC algorithm.

hello, I am using P-NUNCLEO-IHM001 package(nucleo-F302R8, STSPIN L6230 motor driver, BR2804 motor 1700kv-1) to performance FOC algorithm. But i did not find Parameters of the motor, could someone let me know where can i find the datasheet or Details ...

Sun1 by Associate
  • 6082 Views
  • 2 replies
  • 0 kudos

Re: Whitepaper - Improve Motor Drive Efficiency

Hi @Camilo LEMOS​ I had to start a new thread, as you've closed the announcement (which is a strange thing to do in a forum).I went for the whitepaper to find out it requires a rather annoying registration procedure. Why can't we use our my.st.com/co...

Resolved! Electric brake function for PMSM motor control

Hi, I am using B-G431B-ESC1 board for tests and MC-SDK 5.Y.2. I have a motor with Hall sensors. Are there any possibilities for braking the motor other than setting a downward speed ramp to 0.I mean regenerative braking methods, and I'm also wonderin...

DTort.1 by Associate III
  • 2146 Views
  • 2 replies
  • 2 kudos

Resolved! Hello I am new to STM32. I want to Use FOC for controlling sensorless motor. Which MPU/MCU can be used for ESC of drone motor?

HelloI am new to STM32. I want to Use FOC for controlling sensorless motor. Which MPU/MCU can be used for ESC of drone motor. I found STEVAL-ESC001v1 can be used as reference design for entry level commercial drone design. Which software I need to do...

VSabn.1 by Associate II
  • 1841 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.